To give you the best possible experience, this site uses cookies. By continuing to use the site, or by staying here, you agree to our use of cookies in line with our Privacy Policy. Learn more including how to manage cookies here.

Diamond Seals

Diamond Seals, named after their geometry, offer many advantages over an O-ring. One of those advantages is lower compressive force. The unique geometry of the seal's tall, thin profile offers the same sealing function of the O-ring, but without the high load on mating substrates. They still use the cost-effective, straight-walled groove geometry, like an O-ring and have a similar amount of designed squeeze to an O-ring. But, because the Diamond Seal has less material, the force needed to compress the seal into the groove is greatly reduced. Compared to a traditional O-ring groove which is more wide than tall, the Diamond Seal groove is deep and narrow. Diamond Seals function at lower hardware loads than O-rings for reduced creep. 

For a full description of all the advantages offered by a Diamond Seal, link to Engineered Solutions Issue 10

The diamond seal groove is 60% narrower than traditional grooves for comparable seal heights. 

Parker Hannifin
O-Ring & Engineered Seals
2360 Palumbo Drive
Lexington, KY 40509
Ph: 859-269-2351
Fax: 859-335-5128
oesmailbox@parker.com
www.parker.com/oes