To give you the best possible experience, this site uses cookies. By continuing to use the site, or by staying here, you agree to our use of cookies in line with our Privacy Policy. Learn more including how to manage cookies here.

Friction

Friction is a complex subject and can be divided into sub-categories that include running friction, breakout friction, wear, lubrication, and more.  The full edition of the Parker O-Ring Handbook contains many details addressing each of these topics, as well as in depth calculations for estimating frictional properties.  

There a many design characteristics that influence frictional forces, including O-ring cross section, percent of compression, hardness, speed, and more.  A full list is shown below:

 

Friction Factors (in order of importance)
To Increase Friction Factor To Decrease Friction
Increase Unit Load (squeeze) Decrease
Increase RMS Surface Finish (metal) Decrease RMS
Increase Durometer Decrease
Decrease Speed of Motion Increase
Increase Cross Section of O-ring Decrease
Increase Pressure Decrease
Omit Lubrication Lubrication Use Lubrication
Decrease Temperature Increase
Decrease Groove Width Increase
Increase Diameter of Bore or Rod Decrease
Decrease Surface Finish (O-ring) Increase
Stretch O-ring Joule Effect* Compress O-ring
Lower Durometer of O-ring Coefficient of Friction # Increase
    Durometer


* Refer to rotary seals.
# A minor factor and should be ignored in design work other than for ultra high speeds.

 

Parker has a number of friction reducing treatments, such as PTFE and ParkerSlick coating which can be very beneficial at reducing installation or break out friction.  Additionally, there area number of specialty compounds which include ingredients such as molybdenum disulfide, powdered PTFE, or proprietary wax.  During O-ring service, these ingredients migrate to the surface with the benefit of reducing running friction.  Some popular internally lubed compounds include:

 

Compound Material Family  
CL172-70 Chloroprene  
E1022-70 EPDM  
E1244-70 EPDM NSF 61 & USP Class VI
N0818-70 NBR  
N1090-85 XNBR "ELF" Extreme Low Friction
V0848-75 FKM PTFE loaded
VA163-80 FKM  

 

 


Parker Hannifin
O-Ring Division
2360 Palumbo Drive
Lexington, KY 40509
Ph: 859-269-2351
Fax: 859-335-5128
ordmailbox@parker.com
www.parkerorings.com